Description From the June 2022 release to the March 2023 release, the Windows 10 hostname will be the default randomized/generated one by Windows, usually something like “DESKTOP-XXXXXXX” instead of the serial number, which either “ERXXXXXXXX” or “CCPXXXXXXXX”. The fix is planned for the March release of 2023. This issue affects images for the following release… Continue reading Windows 10 Hostname
Tag: Hostname
Axis Cameras using HTTPS With a Hostname
Description Axis Cameras running Firmware 9.0 and above fail to connect and stream video when configured to use a hostname instead of IP address and the protocol in the exacqVision Client has been set to HTTPS Required. Product Steps to Reproduce In the exacqVision Client: Go to Add IP Cameras. In the Hostname/IP Address field,… Continue reading Axis Cameras using HTTPS With a Hostname