Onvif with incorrect profile parameter in host name would crash server

Description Onvif plugin does allow additional parameters in the host name for added supports. Such as profile/tranport settings(#Profile=1 or #transport=udp). Profile expects a number but would crash the server if a string is entered. <br> Version Introduced r38461 <br> Platform All <br> Steps to reproduce connect onvif camera with host name and profile with string.… Continue reading Onvif with incorrect profile parameter in host name would crash server