Dewarping of Axis hemispheric cameras does not work through web service

Affected platforms exacqVision web service 7.4 <br> Symptom The Axis dewarping library uses OpenGL and therefor will not work when launched as a Windows service or without access to X Windows in Linux. <br> Workaround Run the webservice as an application rather than a service. In Windows:1. Start => Run cmd enter2. Run the command… Continue reading Dewarping of Axis hemispheric cameras does not work through web service