Description The Host Bus Adapter (HBA) cards have a series of jumpers in place that should not be moved. See below pictures for proper jumper placement.
Tag: HBA
How to Replace a SIIG SC-SA0R11-S1 HBA with an LSI 9300 HBA
Steps Follow the steps below to replace your SIIG SC-SA0R11-S1 Host Bus Adapter card with the LSI 9300 Host bus adapter. <br> Power down the system.Locate the host bus adapter. If your system is a Hybrid with an analog capture board, the host bus adapter is the one with the SATA cables between this card… Continue reading How to Replace a SIIG SC-SA0R11-S1 HBA with an LSI 9300 HBA