Description The audio is not working on the Exacq server and is giving a message “PA_OpenStream (-9996) Invalid device.” Solution The issue is a failed sound card, so it needs an RMA to replace the motherboard or install another sound card
Tag: Hardware Issues
Exacq Storage Issues
Drives failing WD Self Test IssueDrive shows failed on the Hardware tab in the exacqVision Storage area.Certain combinations of exacqVision and other read/write data could cause the Western Digital Drive Short Test (WD DST) to intermittently get stuck in a loop and write excessively to a specific physical drive location dedicated for testing, which causes… Continue reading Exacq Storage Issues