Exacq Mobile Application Views show Black Box

Description  There are a few reports of customer having no live streams in the views created. When selecting the view to monitor some of the live streams show a black box. This has been seen on view containing 4 live streams as well up to 25 streams. Please note that our application only decodes up… Continue reading Exacq Mobile Application Views show Black Box

FLIR Camera Motion Stops Recording Motion Events

Description  Motion will stop working on FLIR models after updating from exacq Server 24.09.5.0 to exacqServer 24.12.7.0. Product  CAMERAS:Flir FC-317-IDFC-324-IDFC-332-ID Steps to Reproduce  Update exacqServer to 24.12.7.0 motion events will stop working properly. Expected Results  Motion should work. Actual Results  Motion Stops working upon updates to 24.12.7.0. Solution Test build exacqVisionServer_24.12.2239205.0_x64 is working25H1 will house… Continue reading FLIR Camera Motion Stops Recording Motion Events

Persistent Event Monitoring in exacqVision Client 25H1

The Persistent Event Monitoring feature in exacqVision Client 25H1 allows users to ensure that event monitoring persists, even if the Client is closed, providing continuous surveillance and notifications of events. The Event monitoring feature in exacqVision has over many years provided a flexible way to bring in situation awareness for the live monitoring use case.… Continue reading Persistent Event Monitoring in exacqVision Client 25H1

Scheduled Exports in exacqVision Client 25H1

This feature included in exacqVision Client 25H1 allows the user streamline the video exporting process by exporting video footage at a scheduled time – for example overnight when the network traffic is minimal. exacqVision allows the user to export video for sharing from it’s search interface. The video from one or more cameras is downloaded… Continue reading Scheduled Exports in exacqVision Client 25H1

Edge Cloud Archiving in 25H1

Support has been added in exacqVision 25H1 for archiving to Amazon S3 or Wasabi target. exacqVision Edge brings the comprehensive capabilities of a VMS to a supported camera, enabling camera-only installs. exacqVision Edge solution avoids the need to have an NVR on premise that needs to be deployed and maintained. The video data was vulnerable… Continue reading Edge Cloud Archiving in 25H1

Live View Search with Remote Connection Sub Streams does not Allow Live Search to Display Search Results

Description  There have been 3 scenarios seen when searching from the live page on 24.12.7.0 Exacq Client if you have Sub Streams enabled.1. If you have remote connection enabled with sub streams searching from live will not return any search results.If you deleted the sub stream it will return search results as expected. 2. If… Continue reading Live View Search with Remote Connection Sub Streams does not Allow Live Search to Display Search Results