Description Customer was getting odd results when trying to edit the name of either a group or username in EM. Product exacqVision Enterprise Manager 21.06exacqVision Enterprise Manager 22.09 Steps to Reproduce From the EM dashboard access either Users or GroupsSelect an existing user or group Click the pencil icon to edit Change the name of… Continue reading Unexpected Results When Updating Groups or Users in exacqVision Enterprise Manager
Tag: Groups
Enterprise Manager Groups
Where are ExacqVision Groups and Views Stored?
Views and Groups are stored on the the relevant ExacqVision servers. For example, if you create a view named “East Side Entrances” that has Camera A from Server 1 and Camera B from Server 2, the group ID and name are stored on both Server 1 and Server 2. Also, Camera A’s membership in “East… Continue reading Where are ExacqVision Groups and Views Stored?
What is the difference between a Group and a View?
Views and Groups are similar in that both of them are logical groups cameras based on more than just the server they are connected to. The major difference is that a View also defines a layout of the cameras onscreen. Because it specifies a layout, the maximum number of cameras in a View is limited… Continue reading What is the difference between a Group and a View?