Yes, ExacqVision Client supports multiple monitors. We have tested up to four VGA monitors from a single workstation.
Typically, a user will run one instance of the ExacqVision Client per monitor. Because decompressing video is CPU-intensive, we recommend one core per Client for the best user experience. To drive up to four VGA monitors, we recommend an Nvidia T1000 graphics card. For always-on, higher end multi-monitor displays consider the Nvidia RTX A-2000 up to the Quadro GV100 discrete graphics cards.
The Nvidia P2000 has been tested running the ExacqVision Client with VGA and DVI monitors up to 1920×1200 resolution.
<br>