Description
exacqVision Server is not detecting motion from Geovision cameras using the onvif plugin. IP camera database indicates motion is supported for the GV-TBL8810
Product
- exacqVision Server 22.09
- Onvif Plugin (onvifnvcpi.json)
- Geovision Cameras
- GV-TBL8810
Steps to Reproduce
- Add Geovision camera to exacq server
- Configure motion on exacq and or the camera
- Trigger motion
Expected Results
- Motion is triggered
Actual Results
- Motion is not triggered in exacqVision
Solution
WARNING – This is temporary and will not survive an upgrade of exacqVision Server Software
Note: See AES-216 for additional information