This procedure is applicable to replacing the primary hard drive of a Linux-based exacqVision system. It assumes that the operating device is installed to an on-board flash device. Do NOT use this procedure when simply adding a drive to a system.
Tag: fstab
Manually Checking a Drive for Errors in Linux
Run fsck On Linux systems, if a disk encounters a filesystem error, the physical drive may still be good but require a file system consistency check. Perform the following steps to attempt to correct this. If the affected volume is a video storage volume: <br> Appendix If drive fails to unmount, you will need to… Continue reading Manually Checking a Drive for Errors in Linux