Overview As part of Exacq’s Remote Connectivity solution, it utilizes the Fast Reverse Proxy Client, known as frpc.exe. This service plays a key role in the remote connectivity solution, enabling users to securely access their NVRs from virtually anywhere. FRPC has been a trusted component in Exacq for some time, having previously been integrated into… Continue reading Fast Reverse Proxy Client (frpc.exe)
Tag: FRPC
Remote Connectivity Fails to Connect to Switchboard
Description When enabling Remote Connectivity for an exacqVision Server on the Remote Connections page within the Client, the Connectivity Status column displays an error. Issue Examine the message displayed in the Connectivity Status column on the Remote Connections page or the exacqVision System Logs. Disabled: SBS: listener stopped 1-CANCELLED May be caused by missing frpc… Continue reading Remote Connectivity Fails to Connect to Switchboard
ExacqVision Web Server Relay Service Issue
Description How to diagnose if the Fast Reverse Proxy Client (FRPC) is the source of issues with the ExacqVision Web Server relay service. Product ExacqVision Web Server Troubleshooting FRPC FRPC provides a proxy service for Relay Connections used by ExacqVision Web Server. This eliminates the need for firewall configuration and prevents exposing the NVR directly… Continue reading ExacqVision Web Server Relay Service Issue