Frequent Restarts on Linux Systems Archiving over Slow Network

Linux-based exacqVision servers could reboot frequently in certain conditions: Linux operating systemActive hardware monitoringArchiving over a slow network (WAN or other network with limited resources) This issue was fixed in version 6.3.33.65575, and it is available in public release 6.4. To work around this issue in affected versions, complete the following steps to configure an… Continue reading Frequent Restarts on Linux Systems Archiving over Slow Network