Description The Cloudvue Gateway video file storage structure is as follows: Product Solution /smartvue/video/MAC/YYYY-MM-DD/EPOCHTIME.mp4 MAC (The MAC address of a connected camera)YYYY (Year such as 2023)MM (Month such as 03 for March)DD (Date such as 30 for the 30th)Note: The folders Year, Month Date are UTC/GMT not the local time zone of the Cloudvue Gateway.… Continue reading Cloudvue Gateway – Video File Naming Format
Tag: Format
H264 / H265 vs JPEG
What are the differences between H.264/H.265 and JPEG? Why would you choose to use one over the other? Learn the answers to these questions in the video above.