Symptom:
Exacq Mobile 3, version 9.2, forces user to re-login to server.
<br>
Problem:
If a mobile user is connected to an exacqVision Server that is on a non-default port (22609), when updating to 9.2 the information stored for that server will be reset. This includes the following:
- Saved login credentials
- History (Last used/Frequently used)
- Security integration login tokens
- Client-side views
- Camera PTZ speed settings
<br>
Solution:
This is a one-time issue. After re-logging into the server all new settings will persist.
<br>