Description With newer Samsung models that supports SUNAPI2. Only the first input trigger is activated for cameras that have multiple trigger inputs. <br> Version Introduced <br> Platform All platforms for IP Cameras using Samsung plugin <br> Steps to reproduce <br> Expected result <br> Actual result Work Around <br> Version Fixed exacqVision Server 8.1.4.102781 <br>