First command to unlock/lock door or other action via Kantech integration fails

Affected platforms exacqVision Server 7.2.0 <br> Symptom When sending a command to an access control module (lock/unlock door, activate/deactivate relays etc.) the first attempt may fail silently. This is likely to happen if the operator credentials are same as the connection credentials. All subsequent commands will succeed or fail with an error message. <br> Workaround… Continue reading First command to unlock/lock door or other action via Kantech integration fails