Description The Cloudvue Gateway video file storage structure is as follows: Product Solution /smartvue/video/MAC/YYYY-MM-DD/EPOCHTIME.mp4 MAC (The MAC address of a connected camera)YYYY (Year such as 2023)MM (Month such as 03 for March)DD (Date such as 30 for the 30th)Note: The folders Year, Month Date are UTC/GMT not the local time zone of the Cloudvue Gateway.… Continue reading Cloudvue Gateway – Video File Naming Format
Tag: Files
Using PSchange to rename files on a remote archive server (Windows)
*** INTERNAL USE *** Description Instructions for how to use PSchange tool in order to manipulate files located on a remote archive server. This guide is for running the tool on a windows OS although it can still manipulate files stored on a linux archive server. Product PSchange.exe Steps net use /delete P: