Adding SCP to Illustra Essentials C2C Cameras

Description  Illustra Essential cameras were manufactured by Topview and do not include scp (Secure Copy Protocol).  As a result, files cannot be easily transferred to or from the device.  The debug.sh script can be used to temporarily install scp onto the device enabling up/downloading of files.  While scp will not survive a reboot the debug… Continue reading Adding SCP to Illustra Essentials C2C Cameras

Using Rsync to Transfer Files to a Cloudvue Gateway

Description  At times it may be necessary to move files to a Cloudvue Gateway and while other tools such as SCP or MobaXterm can usually manage the job, rsync can track progress and resume after an interruption which can be particularly useful when transferring large files like the latest Cloudvue software or on slow or… Continue reading Using Rsync to Transfer Files to a Cloudvue Gateway