Title Running Windows Chkdsk Command Description Chkdsk, also known as Microsoft Check Disk, is a utility that can be used in almost all Windows versions. The Chkdsk commands used to scan through entire hard drives to find and fix any errors. Chkdsk should be run whenever file system corruption is suspected whether by odd behavior… Continue reading Running Windows Chkdsk Command
Tag: File System
How to Determine Whether a File is Bookmarked
NOTE: For better understanding of this article, you should be familiar with the basic filename format for exacqVision data (see https://exacq.com/kb/?crc=30471).A file is known to contain bookmarked content if: The filename plugin ID (XXXX in the file name) matches the device manufacturer’s ID (list of available IDs: https://exacq.com/kb/?crc=30471).The device number (YY in the file name) matches the camera’s… Continue reading How to Determine Whether a File is Bookmarked
What file systems does ExacqVision support?
File systems supported by ExacqVision are as follows: <br> Windows: Ubuntu/Linux: <br> Using file systems other than those listed may result in data loss, inability to recognize storage volumes, incompatibility when updating to future software versions. <br>