Accessing exacqVision from Tablets and Phones using the exacqVision Mobile App

Overview exacqVision Mobile receives live and recorded video from the exacqVision Server The exacqVision Mobile app allows you to use Apple or Android tablets and smartphones to view live video from an exacqVision Server, search for recorded video, and more. To access your exacqVision server over the internet from exacqVision Mobile, additional configuration may be… Continue reading Accessing exacqVision from Tablets and Phones using the exacqVision Mobile App

Top 10 Illustra Camera Questions

What is the default IP address and credentials?192.168.1.168, admin/adminUnable to adjust Zoom on Camera?Windows XP/7 and IE7/8/9/10/11 Clean IE cacheAdd IP to Trusted siteJava Settings , lower security to MediumAdd IP to Compatibility ViewMake sure to install active X and accept java when promptedCamera picture Off set on Illustra 200/210/600/610Add IP address to compatibility viewZoom… Continue reading Top 10 Illustra Camera Questions

Motion Not Recorded

Are you seeing colored borders around the live video panels in the exacqVision Client when motion appears to be occurring? <br> Yes: Go to the Camera Time section below.No: Go to the Motion Area section below. NOTE: If the camera is configured to detect motion and also configured for Free Run recording on its schedule… Continue reading Motion Not Recorded

Accessing exacqVision from Tablets and Phones using the Exacq Mobile 3 App

NOTE: This article is a reference for Legacy Exacq Mobile 3 users. Users capable of upgrading their exacqVision Server to version 24.09 and higher should refer to the article: Accessing exacqVision from Tablets and Phones using the exacqVision Mobile App on using the exacqVision Mobile app. Exacq Mobile 3 receives live and recorded video from… Continue reading Accessing exacqVision from Tablets and Phones using the Exacq Mobile 3 App