Description Dahua plugin which also supports Illustra Essentials failed to set the NTP server on the camera during initial connection time. By default if there is no override ntp server, the plugin should push the address of the server as NTP on the camera. <br> Version Introduced r71495 (dev build 6.5.38.71503/RC build 6.6.0.71575) <br> Platform All… Continue reading Dahua/Illustra Essentials plugin failed to post NTP server address on the camera at startup.