Servers are able to be enabled if Web Service initialization fails

Description When connecting to a web service whose initialization fails, all servers should be disabled. <br> Version Introduced 8.0 <br> Platform All <br> Steps to reproduce Add a web service that causes initialization to fail. <br> Expected result The enable toggles for each server on the web service is disabled. <br> Actual result The enable… Continue reading Servers are able to be enabled if Web Service initialization fails

Toggling a Web Service Connection Multiple Times Can Cause Failed Initialization

Description Enabling and then Disabling a Web Service multiple times within Exacq Mobile 3 during the connection process can prevent the servers from being retrieved. <br> Version Introduced <br> Platform Mobile-All <br> Steps to reproduce <br> Expected result The Server List is displayed <br> Actual result The Text ‘Unable to retrieve servers’ is displayed <br>… Continue reading Toggling a Web Service Connection Multiple Times Can Cause Failed Initialization

Panels repopulate after clearing on server initialization failure

Description After opening the application if the panels are cleared before a server initialization fails the panels are repopulated. <br> Version introduced <br> Platforms Mobile – All <br> Steps to reproduce On Exacq Mobile 3 <br> On Browser <br> Expected result The panel(s) remain cleared <br> Actual result The panel(s) are repopulated <br> Workaround Clear… Continue reading Panels repopulate after clearing on server initialization failure

notifypi – failure to send email on falling edge

Description A NotifyPI enhancement was released with 8.4 which added the ability to specify ‘when’ to send an email: ‘Alarm Starts’, ‘Alarm Ends’ or ‘Alarm Starts and Ends’). However, the ‘Alarm Ends’ selection was failing to send the email when the trigger event (alarm) duration was shorter than the ‘Send Rate Limit’.If the event duration… Continue reading notifypi – failure to send email on falling edge