Axis V5915 audio-out fails in digest authentication mode.

Description Audio-out does not work with V5915 fw 5.75.1.4 and set to digest or basic or digest authentication mode. This is a misbehave camera fw that server 8.4 does not support properly. Work around is either revert back to 8.2 or set the camera to basic authentication mode until the issue is fixed. <br> Version… Continue reading Axis V5915 audio-out fails in digest authentication mode.