Symptom When starting a system from power-off the tDVR board fails to initialize, causing one or more of the following symptoms: Blinking red LED lights near the processor.Device Manager misreporting an 8008, 8016, or half of an 8032 as hardware ID 8000 in the Device Properties detailt tab.Ispci not listing an Exacq Technologies 8008, 8016,… Continue reading tDVR board fails to initialize after cold starting a system