Issue When system reboots and boots up to recovery mode it selects “Factory Capture” by default leading the system to commit a full factory restore upon pressing “enter”. Solution Windows <br> Linux System The file at ‘/boot/efi/EFI/BOOT/refind.conf’ will need to be edited in the same way it is for the Windows instructions. Instead we would… Continue reading System Unexpectedly Reboots Into Recovery Mode Then Enters Factory Restore
Tag: Factory Restore
System Recovery using on-board recovery partition
Exacq systems built after 10/17/2015 include a special partition to allow for quick and easy system restoration to factory default conditions. This recovery will only affect your operating system drive. <br> To start the Recovery, during system boot up, prior to loading the operating system, press the “S” key on your keyboard. You will be… Continue reading System Recovery using on-board recovery partition