Reboot or Default a Camera from the exacqVision Client

Description  Prior to the release of exacqVision Client Version 22.03 cameras could not be rebooted or factory restored via the Client.  With the introduction of the Camera Web Configuration feature, cameras can now be rebooted or factory reset from within the Client.    Product  Solution <br>

Factory resetting the bios for G-Series Micro

IMPORTANT: This article reflects G-Series Micros built prior to mid-2024. To factory reset the bios for G-Series Micro, you need to follow these steps:- 1-Unplug power cable from the Unit 2-Remove the 4x Phillips Chassis screws 3-Remove bottom and top cover 4-Remove the RAM stick 5-Plug in power cable (should turn on automatically), and Wait… Continue reading Factory resetting the bios for G-Series Micro

Factory default E-Series encoders not discoverable on Una LC-Series server

Affected platforms Una LC-Series with exacqVision 7.2 <br> Symptom Factory default E-Series encoders are discoverable through UPnP on the same subnet, but do not respond to WS-Discovery requests across subnets unless a DHCP server is present. On an Una POE port a DHCP server does not exist, so discovery only works on the same subnet,… Continue reading Factory default E-Series encoders not discoverable on Una LC-Series server

System Recovery using on-board recovery partition

Exacq systems built after 10/17/2015 include a special partition to allow for quick and easy system restoration to factory default conditions. This recovery will only affect your operating system drive. <br> To start the Recovery, during system boot up, prior to loading the operating system, press the “S” key on your keyboard. You will be… Continue reading System Recovery using on-board recovery partition