Description
Setting a Record Video via Video Motion Event will not clear on an Axis Q6114-E camera running Edge software.
<br>
Tested Version
Edge 7.6.1.93449
Firmware 6.20.1
Client 7.6.4.94409
<br>
Platform
Edge
<br>
Steps to reproduce
- Set a Motion Window on the camera via the Client
- Confirm Motion Detection is functional
- Create a new Event in Event Linking – Video Motion > “Motion Test” > Record Video > Pre set to 1 > Post set to 1 > Apply
- Trigger motion on camera
<br>
Expected result
- Motion triggers a red border based on the Event. The event should clear 1 second after motion has ceased being detected (based on Post-Trigger timing).
<br>
Actual result
- The red border only clears when the 127.0.0.1 input is disconnected and re-connected to the Edge server.
- Deleting the Event while the border is present does not clear the border.
- Setting the schedule to Event Only has no effect.
- Soft Triggers still function as expected
<br>
Fixed Version
7.9.16.99811