Best Practice for Expanding an Array Using NTFS (Windows)

With hard drive offerings only increasing in size, it is important to remember that some large increases in RAID Arrays may not be read correctly by Windows. This is because there are limits to the cluster size that different sizes of volumes can use. If the volume is expanded beyond a cluster size limit, it… Continue reading Best Practice for Expanding an Array Using NTFS (Windows)