Are All ONVIF-conformant Cameras Compatible with ExacqVision Systems?

The streaming profile of ONVIF (Profile S) provides a standard interface for streaming video and audio between conformant devices (cameras or encoders) and clients (VMS). The ExacqVision VMS is listed as anĀ ONVIF Profile S-conformant client. Extensive testing with a wide variety of ONVIF Profile S-conformant cameras has revealed enough inconsistency that Exacq does not explicitly… Continue reading Are All ONVIF-conformant Cameras Compatible with ExacqVision Systems?

Replacing XDVR drivers with SDVR drivers on Linux-based exacqVision Systems

If you have an Linux-based exacqVision system (such as exacqVision EL) that requires SDVR drivers, but you mistakenly installed XDVR drivers, you must remove the XDVR drivers before installing the SDVR drivers. There are two equal ways to remove the XDVR drivers; use the one that you prefer or have better access to: In Terminal,… Continue reading Replacing XDVR drivers with SDVR drivers on Linux-based exacqVision Systems

No Audio from PC Speaker on Linux-Based exacqVision Systems

If you cannot hear audio on Linux-based exacqVision (eV) systems, try adjusting the volume setting on the front speaker (the default setting is for this volume is zero). To adjust the volume setting, complete the following steps: Exit the eV Client software and log out of the user account.Log in to Linux using an administrator… Continue reading No Audio from PC Speaker on Linux-Based exacqVision Systems

Default Windows User Accounts on Exacq Systems

When setting up a new Exacq system, the out-of-box experience will prompt you to create a default operating system account. This account will be given administrative privileges. Additional user accounts may be created using the Kiosk scripts available on the Desktop. Kiosk user accounts have restricted privileges. The Kiosk account is blocked from all operating… Continue reading Default Windows User Accounts on Exacq Systems