To view the article “Identifying the Motherboard Installed in an exacqVision System,” please open the attached PDF.
Tag: exacqVision System
Throttling Issues After Changing the Storage Configuration on an exacqVision System
Before troubleshooting an exacqVision system that is experiencing throttling, it is important to know how the software writes video to the disk. <br> Each time PSFPI attempts to open a record stream, the disk volumes are checked for available space. The available space is determined by adding 1GB to the currently used space. The volume… Continue reading Throttling Issues After Changing the Storage Configuration on an exacqVision System
Using External USB DVD Drives with an exacqVision System
External USB DVD drives can be connected to an exacqVision system if they are compatible with the operating system (Windows 7 or Ubuntu 10.04 Linux). Although third-party USB DVD drives are not specifically supported or certified for use with exacqVision systems, Samsung SE-S084D/TSBS and LG GP08NU6B DVD drives have been successfully used for this purpose.… Continue reading Using External USB DVD Drives with an exacqVision System