Why doesn’t my ExacqVision system capture the exact frame rate configured for my camera?

The Frame Rate setting on the ExacqVision Camera Recording page, or the individual Camera Settings page, is a requested setting; this frame rate is not guaranteed. Although the ExacqVision software is designed to capture every frame that it receives from the camera, the actual recorded frame rate can be reduced by network issues, firmware, scene… Continue reading Why doesn’t my ExacqVision system capture the exact frame rate configured for my camera?

Bad Package Quality Error when Installing exacqVision Software on Ubuntu 11.04

Exacq recommends installing exacqVision software on Ubuntu 10.04 because of its extensive testing within the Ubuntu community and its status as a Long Term Support version. However, if you try to install exacqVision Client and exacqVision Server software version 4.5 and older, exacqVision Web Service, or Enterprise Health Manager on a Ubuntu 11.04 system, the new Ubuntu Software Center… Continue reading Bad Package Quality Error when Installing exacqVision Software on Ubuntu 11.04

RTSP Plug-in used with ExacqVision Software

The RTSP plug-in supports generic streaming of audio and video using the RTSP/RTCP/RTP protocol. The plug-in automatically configures the streaming transport to either UDP or TCP. The default when the device is connected is TCP; if it fails to connect, it tries to connect through UDP. The plug-in does not support any configuration — it… Continue reading RTSP Plug-in used with ExacqVision Software