In various versions of exacqVision, version 8.8 and earlier, we have seen issues updating the IP settings on Linux servers using the exacqVision client. If you run into this issue, you can confirm the settings applied or change the settings using the method below. The exacqVision Client reads from the Interfaces file so if this… Continue reading Issues Updating IP Settings using the exacqVision Client
Tag: exacqVision Servers
Enabling Audio Line Inputs in Linux
By default, Line In is not enabled in Linux. To enable Line In, complete the following steps:<br>Open a Terminal window and run alsamixer. This opens a window that allows you to change settings for each sound channel.<br> Press the F4 key to change capture settings. <br> Use the left and right arrow keys to select capture… Continue reading Enabling Audio Line Inputs in Linux
exacqVision SDK Compatibility with exacqVision Server Versions
The exacqVision SDK is designed to be compatible with all versions of exacqVision Server. However, individual features in certain versions of the server and SDK might not be compatible. For more details about the features available in a each version of the server or SDK, see the readme.txt file available in their install packages. It… Continue reading exacqVision SDK Compatibility with exacqVision Server Versions
RAID Setup Using 3ware Controller – LEGACY
To configure a RAID 5 array using a 3ware controller, complete the following steps: <br> Restart the computer.When prompted, press Alt-3 to enter the 3ware RAID BIOS.If prompted, type admin256 as the password.Press any key to acknowledge the warning.The available drives are listed under Exportable Units. If you are re-creating a failed RAID array, some drives will… Continue reading RAID Setup Using 3ware Controller – LEGACY