exacqVision Drive Setup with 3Ware (JBOD)

Part I: Enter the 3Ware BIOS Restart the system through the operating system.When prompted, press Alt+3 to enter the 3ware RAID BIOS.Type admin256 as the password.Press any key to acknowledge the warning. <br> Part II: Create the New Array Press the Tab key to navigate to the top of the list of drives listed as Exportable Unit. Highlight single drive under Direct Attached and… Continue reading exacqVision Drive Setup with 3Ware (JBOD)

RAID Setup Using 3ware Controller – LEGACY

To configure a RAID 5 array using a 3ware controller, complete the following steps: <br> Restart the computer.When prompted, press Alt-3 to enter the 3ware RAID BIOS.If prompted, type admin256 as the password.Press any key to acknowledge the warning.The available drives are listed under Exportable Units. If you are re-creating a failed RAID array, some drives will… Continue reading RAID Setup Using 3ware Controller – LEGACY