Exacqd handle leak

Symptom: It is possible after a very long period for the server to stop functioning, requiring a restart. Problem: There is a slow handle leak in exacqd introduced in server version 9.5.25/9.6.0. This handle is never used, so a slow memory leak is the result.  Windows has a limit of 16 million handles. A server… Continue reading Exacqd handle leak

SCN-00000008 – Privileged ‘exacqd’ process

SCN #SCN-00000008Title of SCNPrivileged ‘exacqd’ processTRAC ##15536Effective Version9.5.25 – Public 9.6Products AffectedServerReason for Change (Summary)CyberProtection requirement that software not run with elevated privileges by default. Change Traditionally, one process runs when the exacqVision Server Service starts: ‘core’ (Linux) or ‘core.exe’ (Windows).  Beginning in 9.6, tasks that require activating a binary or script will be moving… Continue reading SCN-00000008 – Privileged ‘exacqd’ process