Description The Camera Recording Page in the client doesn’t show any of the default options such as, IP Address, Camera Name, Video Detection, Record Status, Last Motion, Mac Address, Type, Model, Firmware. Product Exacq Client 23.06 and as early as 22.12 Steps to Reproduce Remove Exacq Vision Client completely from the Recorder, or any client… Continue reading Camera Recording Page Columns Missing on Fresh Install