In the ExacqVision Edge Server Trunk build version 21.06.114, We have improved our config persistence algorithm to guard against sudden power losses. you can download and use this version or wait until the next official release which is 21.09
Tag: Exacq Edge
exacqVision Edge Time Zone Configuration
exacqVision Edge is a version of exacqVision Server that runs directly on supported camera models and only connects to, and records video from, the camera it is hosted on. Cameras running the exacqVision Edge, or Edge+, application must be configured for the GMT+0 time zone. Because the server application runs directly on the camera, the… Continue reading exacqVision Edge Time Zone Configuration