Description When installing the Pelco NET 6516 encoder and using Exacq server version 24.12, you may experience interruptions in the footage. Steps to Reproduce Install Pelco encoder NET 6516 with Exacq server 24.12.0 to 24.12.7 Expected Results You should see footage without any interruptions from the playback. Actual Results You will see interruptions in the… Continue reading The Pelco NET 6516 encoder experiences interruptions in the footage when used with Exacq Server version 24.12
Tag: Exacq
Exacq AV1 Codec Support
Description Exacq are in the process of adding support for the AV1 Codec. AOMedia Video 1 (AV1) is an open, royalty-free video coding format initially designed for video transmissions over the Internet. It was developed as a successor to VP9 by the Alliance for Open Media (AOMedia),[2] a consortium founded in 2015 that includes semiconductor firms, video on demand providers, video content producers, software development companies and web browser… Continue reading Exacq AV1 Codec Support
Hikvision Camera losing motion / stops recording
Description This resolves the issue where the camera recording is stopped on motion recording schedule. The user then has to disable and re-enable the camera for it to start recording again. Product Exacq Server Solution User has to upgrade to 22.12 or later.