exacqVision Hard Drive Tests

Description  A summary of system drive tests performed by exacqVision using evSelfTest, RAID controllers, and S.M.A.R.T. data. Product  Information On systems Built-by-Exacq (BBE), the exacqVision software runs the following tests: Using evSelfTest.exe: RAID card consistency check, once every week.On non-BBE systems:

For Debugging Purposes, The Logging of Additional Information Related to the Storage Self-Tests May Be Enabled.

Starting with server version 19.08, it is now possible to collect additional information about storage self tests. evselftestYYYY-MM-DD.txt files in the server/logs path will trace all of the commands that evselftest issues along with their corresponding output. This feature is turned on when the EvselftestLogEnabled attribute under “Storage” is set to “1” in sysmgmtpi.xml.

2021-02 – Hard Drive Issues Training

Hard Drive Issues Troubleshooting

Manually executing evselftest

Description evselftest binary location Windows 32-bithttps://svn.exacq.com:8443/!/#3PV/view/head/exacq/evselftest/tags/1.0.0.97921/Windows_x86_vc9Windows 64-bithttps://svn.exacq.com:8443/!/#3PV/view/head/exacq/evselftest/tags/1.0.0.97921/Windows_x64_vc9Linuxhttps://svn.exacq.com:8443/!/#3PV/view/head/exacq/evselftest/tags/1.0.0.96435/Linux_x86 command help admin@exacqVision-Server:/tmp$ sudo ./evselftest Supported options: -h [ –help ] show help -c [ –cmd ] arg self-test command to execute. supported options are startshort, startlong, stop, report -d [ –disk ] arg [optional] – disk on which self-test command to execute. If this option is missing,… Continue reading Manually executing evselftest