Exacq Scenario Series – Illustra IQ Perimeter Object Classification to Change ExacqVision Views

The Scenario Series of videos addresses setup configurations for specific use cases. In this video our scenario is that of a user that wants to use Event Monitoring to bring attention to an ExacqVision operator when a perimeter area is crossed. This could be used to monitor property and fence lines. We walk through setting… Continue reading Exacq Scenario Series – Illustra IQ Perimeter Object Classification to Change ExacqVision Views

Enabling Exacq Mobile 3 Push Notifications

Push notifications provide the ability to alert users of events even when they do not have the Exacq Mobile 3 app open. There are two options for Push Notifications, those triggered by camera analytics and analytic appliances, and those triggered by other types of events, which require the use of Event Monitoring. Both options are… Continue reading Enabling Exacq Mobile 3 Push Notifications

Scenario Series – Illustra IQ Object Classification to Change ExacqVision Views

<br> The Scenario Series of videos addresses setup configurations for specific use cases. In this video our scenario is that of a user that wants to use Event Monitoring to bring attention to an ExacqVision operator when someone parks in specific parking spaces. This could be used to prevent people from parking in forbidden areas,… Continue reading Scenario Series – Illustra IQ Object Classification to Change ExacqVision Views

The Event monitoring trigger is not switching the video

The Event monitoring trigger is not switching the video Description The Event monitoring trigger is not switching the video the first time if you run it while another trigger works. Reproducing the issue:- creating Two event monitoring profiles using the Video Panel/View type and setting two soft triggers to trigger it manually, then set the… Continue reading The Event monitoring trigger is not switching the video

Event Monitoring is not Allowing the Analytical Event Source to be Created and Reverts to Tampering

Description  If you are exhibiting an event monitoring rule for analytical Event Source of any type you can not save the event rule IF your SYSTEM name of the NVR is the SAME name as the Event Source Device. Product  Steps to Reproduce  Go to Event Monitoring and set the rule up. Expected Results  The… Continue reading Event Monitoring is not Allowing the Analytical Event Source to be Created and Reverts to Tampering

Web Service event monitoring information not provided

Description Retrieving event monitoring information from the web service is broken in 8.4. Currently, requests to eventmonitoring.web will return an empty profile list, independent of any configured event monitoring profiles. Note: This directly affects the registration and receiving of push notifications in mobile. <br> Version Introduced <br> Platform Web Service / All <br> Steps to reproduce <br>… Continue reading Web Service event monitoring information not provided

Customizing Client Audio Alerts

The ExacqVision Desktop Client software has the ability to alert users with audio when using Event Monitoring. See the Client Help file, press F1, to learn how to set up Event Monitoring, or watch the Event Monitoring training video.Using audio alerts is a good way to bring attention to system operators when events of importance… Continue reading Customizing Client Audio Alerts

Configuring Views that Change Based on Events

Introduction A useful feature of exacqVision Client is to automatically switch to a view that highlights an event in progress. This can be configured two slightly different ways in exacqVision Client: <br> Configuration Steps Each of these methods are explained in the following sections. Configuring Event Monitoring using a Default View and the Event Monitoring… Continue reading Configuring Views that Change Based on Events