Description Setting a Record Video via Video Motion Event will not clear on an Axis Q6114-E camera running Edge software. <br> Tested Version Edge 7.6.1.93449Firmware 6.20.1Client 7.6.4.94409 <br> Platform Edge <br> Steps to reproduce Set a Motion Window on the camera via the ClientConfirm Motion Detection is functionalCreate a new Event in Event Linking –… Continue reading Axis plugin motion detection alarm event might not expire