How to: Using EVAPI_Callback and EVAPI_CallbackEx

Overview The evAPI callback functions are used to receive event notifications from the exacqVision server, such as motion detected by a camera or a configuration change made to a server. Usage To use the evAPI callback functionality, it is necessary to define and declare a callback function and then assign the function in the API.… Continue reading How to: Using EVAPI_Callback and EVAPI_CallbackEx