Categories
Knowledge Support Support exacqVision Enterprise Categories Products

Disabling or enabling of a camera will cause ESM importer to crash

Affected platforms

ESM version 3.6.1, trunk builds 3.7.3 through 3.7.5

<br>

Symptom

When a camera is enabled or disabled in the exacqVision client, ESM backend will crash. In the UI in the upper right corner, you will notice servers dropping and reconnecting. Inspection of importer log will show the crash.

<br>

Workaround

Do not disable/enable cameras

<br>

Resolution

Update ESM to version 3.6.2 or later (excluding the 3.7.3 – 3.7.5 trunk builds)