ESM returns error when entering a rule duration using a decimal

Affected platforms ESM 3.2 or later <br> Symptom If the user enters a value using a decimal (for example, 10.5) for the duration value of a rule, ESM returns an error page when the user attempts to create the rule. <br> Workaround Enter a valid integer (not a decimal number) between 1 second and the… Continue reading ESM returns error when entering a rule duration using a decimal