Description This error has been observed when adding illustra cameras to a Cloudvue Gateway. Product Steps to Reproduce Expected Results Actual Results Solution
Tag: Error Message
Systems MAC Address is Currently Locked Out
Description When attempting to import a license key using the Import From exacq.com option, an error message “This systems’s MAC address is currently locked out.” is displayed. Product exacqVision ClientexacqVision Server Steps to Reproduce From the Configure System page (Configuration > YOUR SERVER > Configure System) select the Import… icon in the License section. Expected… Continue reading Systems MAC Address is Currently Locked Out
exacqVision sysprep Error “Failed to Write Model number”
Title exacqVision sysprep Error “Failed to Write Model number” Description During a full re-image of an exacqVision Server, while doing the sysprep, an error occurred “failed to write the model number” (see Figure 1) Product exacqVision Server Solution It was discovered that the integrator was using the wrong iso file for the… Continue reading exacqVision sysprep Error “Failed to Write Model number”
Axis Displays “Device Reporting an Error”
Problem: An Axis camera may display the error “Device reporting an error, the device reported that is has encountered an error (500)” but continues to display a normal video stream. <br> Explanation: This is typically caused by a camera that does not have native PTZ functions but could be connected to an external PTZ device… Continue reading Axis Displays “Device Reporting an Error”
dpkg-reconfigure causes a false-negative error message
Description Why would someone ever want to execute dpkg-reconfigure when edvrserver already installed? To re-execute any of the following postinst actions: Update nsswitch.conf for our mDNSresponder.Configure rp_filter for camera discovery.Restore MISSING streampi.xml. (reminds me of a factory default)Restore MISSING useraccounts.xml. (reminds me of a factory default)Make pulse audio system-wide.And of course, if you want to… Continue reading dpkg-reconfigure causes a false-negative error message