HTTP Response Code Reference

Code Description Definition Exacq Tips Informational 100 Continue Server received request, client should continue. 101 Switching Protocols Response to upgrade header 102 Processing Server processing received request. 103 Early Hints Used with link header.Allows browser to preload resources. Successful 200 OK Standard response for successful request.Meaning varies based on method (GET, POST, etc). 201 Created… Continue reading HTTP Response Code Reference

Server 23.09 Fails to Run on Ubuntu 14.04 x86

Description Users with Ubuntu 14.04 x86 (32-bit) experience an error when attempting to install or update to ExacqVision Server version 23.09. <br> Product ExacqVision Server 23.09 x86 and above <br> Steps to Reproduce Attempt an update or fresh install of ExacqVision Server version 23.09 on a Ubuntu 14.04 x86 system. <br> Expected Results Installation without… Continue reading Server 23.09 Fails to Run on Ubuntu 14.04 x86

Directory Could Not be Created – Symbolic Linking Error 17

When exacqVision Client starts, it looks for a folder named “exacqVision Files” inside the directory of the currently active user. If it doesn’t find one, it creates the directory for exported video. On exacqVision systems, the masterscript creates a symbolic link here that directs data to the “/mnt/export/admin” directory so that exported video does not… Continue reading Directory Could Not be Created – Symbolic Linking Error 17

“Failed to write fstab” Error Displayed while Configuring S-Series Partitions

Symptom A “Failed to write fstab” error can appear if the system is running low on space on the root “/” partition. <br> Affected Versions This affects all exacqVision S-Series versions. A fix will be released at a later date. <br> Resolution To recover from this error, free up space on the root partition using… Continue reading “Failed to write fstab” Error Displayed while Configuring S-Series Partitions

ESM returns error when entering a rule duration using a decimal

Affected platforms ESM 3.2 or later <br> Symptom If the user enters a value using a decimal (for example, 10.5) for the duration value of a rule, ESM returns an error page when the user attempts to create the rule. <br> Workaround Enter a valid integer (not a decimal number) between 1 second and the… Continue reading ESM returns error when entering a rule duration using a decimal

exacqCloud dashboard search for server name returns error page

There are occasions when a server name search on the dashboard on ESM returns an error page with “contact administrator” message. <br> If this happens get the esm logfiles.open logfile-websevice fileverify that this log file has the messages “ProtocolError: (‘Connection aborted.’, error(111, ‘Connection refused’))” If the message above is in the log file, restart the… Continue reading exacqCloud dashboard search for server name returns error page

Line Expected Mac Client Error

Problem When opening the Mac client the user sees an error dialog box appear stating something similar to “file, line X: ‘-‘ expected”. This is caused by a corrupted client configuration. <br> Steps to fix Close the exacqVision client.Open “Finder” from the Mac desktop.From the desktop menu bar, open the “Go” menu and select “Go… Continue reading Line Expected Mac Client Error

exacqVision Client Error – Unable to exclusively lock file

Symptom   Problem When viewing cameras, the user would occasionally see the following exacqVision Client Error message: It was observed that the C:\ProgramData\boost_interprocess\ folder is being renamed by software running in their corporate environment. The exacqVision Client uses the boosts IPC folder which is sometimes used by the other software. Example After a reboot it… Continue reading exacqVision Client Error – Unable to exclusively lock file