Description The C2C Gateway video file storage structure to the local SD card is as follows: Product Solution /media/sd1/videos/YYYY-MM-DD/EPOCHTIME.mkv YYYY (Year such as 2023) MM (Month such as 01 for January) DD (Date such as 30 for the 30th) Each directory (YYYY-MM-DD) contains video files recorded that day, each video file uses the naming naming… Continue reading Cloudvue C2C – Video File Naming Format
Tag: Epoch
Cloudvue Gateway – Video File Naming Format
Description The Cloudvue Gateway video file storage structure is as follows: Product Solution /smartvue/video/MAC/YYYY-MM-DD/EPOCHTIME.mp4 MAC (The MAC address of a connected camera)YYYY (Year such as 2023)MM (Month such as 03 for March)DD (Date such as 30 for the 30th)Note: The folders Year, Month Date are UTC/GMT not the local time zone of the Cloudvue Gateway.… Continue reading Cloudvue Gateway – Video File Naming Format