ePlayer failing to load dewarping libraries

Description ePlayer is failing to load dewarp libraries <br> Version Introduced 7.9.20 <br> Platform Windows <br> Steps to reproduce Create an exe export from the client for any fisheye cameraOpen the exe export <br> Expected result ePlayer should be able to dewarp the video <br> Actual result ePlayer is not able to dewarp the video… Continue reading ePlayer failing to load dewarping libraries

exacqVision Export Video File Types

Video may be exported from exacqVision in different formats. The table below illustrates some of the differences in these formats. Multi-Camera: For the purposes of this article, multi-camera means many camera streams are combined into a single exported file. When exporting as .MOV, .AVI, or .MP4 each stream will end up as its own file.… Continue reading exacqVision Export Video File Types

How do I save a video clip to an executable file that I can send to the police?

The ExacqVision Desktop Client application can be used to export video and audio to an .EXE executable file which packages the ExacqVision ePlayer with it to become a self-playing file. The fact that the .EXE export has the ePlayer packaged with it makes it ideal for sharing with law enforcement who may not have access… Continue reading How do I save a video clip to an executable file that I can send to the police?