Integrating exacqVision with a Kantech EntraPass installation that uses EntraPass Web may prevent use of EntraPass Web, or vice versa.

Affected platforms exacqVision 7.4 with EntraPass 6.05.02 or newer <br> Symptom By default EntraPass only allows a single connection to EntraPass Web. When exacqVision is integrated with EntraPass Web, it consumed a connection EntraPass Web. If EntraPass Web then attempts to connect, it will fail. Likewise, if EntraPass Web is connected first, exacqVision will fail… Continue reading Integrating exacqVision with a Kantech EntraPass installation that uses EntraPass Web may prevent use of EntraPass Web, or vice versa.

Kantech Entrapass Web Download Instructions

Instructions: ExacqVision Kantech-Onboard systems may exhibit specific Internet Explorer security settings that will prevent the download of EntraPass Web from the link on the desktop after installing the Kantech software. This was discovered specifically with the Windows Server 2016, Entrapass version 7.51, in June 2019. Other versions may encounter this problem though they are not… Continue reading Kantech Entrapass Web Download Instructions

Create a Report in Entrapass Web

Description There are four types of reports available:* Quick Reports filters events such as access, time, attendance, doors, logins, operations, etc.* User List filters cards such as card type, card number, username, company, department, etc.* Component List filters access levels, doors, controllers, relays, inputs, etc.* Custom Reports schedules and automates future dates. <br> Entrapass Web… Continue reading Create a Report in Entrapass Web

Create a Map in Entrapass Web

Description Creating maps allow you to visually interact with all system components such as:relays, inputs, outputs, keypads, elevators, doors, cameras, workstations, sites, gateways and controllers.This diagram illustrates a typical Kantech Entrapass Server and System Component architecture.<br> Entrapass Web Navigate to the Operation menu and select MapClick Add button.Give the new map a name.Click in box on left side and select Change… Continue reading Create a Map in Entrapass Web

Override a Holiday in Entrapass Web

Description Holidays ignore proper access levels of all users and assigned unlock schedules of all doors.You can override a holiday by scheduling an exception for a user or door.<br> Entrapass Web Navigate to the Configuration menu and select Schedule Select Site to schedule the exception. Select desired Door Unlock Schedule, then click Edit to override. Place a check mark in holiday to override.… Continue reading Override a Holiday in Entrapass Web

Add a Holiday in Entrapass Web

Description Access and schedules for a particular date are ignored when a day is designated as a holiday.You can program a holiday to disregard proper access levels and door unlock schedules.<br> Entrapass Web Navigate to the Configuration menu and select Holiday Click Add button. Fill in details of new holiday. Select date of new holiday. Drag Sites into Holiday Type. <br>

Create an Access Level in Entrapass Web

Description The security of employees and properties depend on managing access.You must create a schedule before defining access levels. <br> Entrapass Web Navigate to the Configuration menu and select Access Level Specify Site for new access level. Click Add button to configure a new access level. Give the new access level a name. Select desired door to assign an existing schedule (cannot… Continue reading Create an Access Level in Entrapass Web

Add a User in Entrapass Web

Description The security of employees and properties depend on managing access.You can create a new card to ensure that a user has proper access levels.<br> Entrapass Web Navigate to the Operation menu and select User Click Add button. Fill in details of new user. Choose Card Type. Type in Card Number. Define proper Access Levels per site. Add Custom Fields or Comments by clicking on… Continue reading Add a User in Entrapass Web

Create a Schedule in Entrapass Web

Description You must create a schedule before defining user access levels and assigning unlock times to doors.The security of employees and properties is achieved by configuring schedules properly.<br> Entrapass Web Navigate to the Configuration menu and select Schedule Specify Site for new schedule. Click Add button to configure a new schedule. Drag the time line pointers to define range of hours. Place… Continue reading Create a Schedule in Entrapass Web