Can’t Set an Email Profile When Kantech Software is Connected to The Exacq Server

Description When having Kantech Board connected to the Exacq Server, Client Software keeps refreshing the configs and that prevents the Exacq client from creating an Email notifications profile. affected version is 23.03 or lower Solution Updating ExacqVision Server and Client to version 24.03 or above. Updating the Kantech Entrapass to version 8.80 or above.

How to Create a User in Kantech for Security Integration with exacqVision

Configuring an Operator to Receive Events from the EntraPass server 1. Login to the Workstation using installer credentials.2. Add a new Workspace (System > Workspace).    a. Select all applications, gateways, controllers, doors, relays, and inputs under their respective tabs.         The screenshots below show the workspace permissions for the ‘exacqws’ workspace.… Continue reading How to Create a User in Kantech for Security Integration with exacqVision