EM failover is not moving the security integration list to the spare server.

Description  When the protected server goes down, and the EM server moves the configs to the Spare server, it will not move the Security integration list to the Spare server. Product  ExacqVision Server 32bit Steps to Reproduce  Installing ExacqVision 32bit version and trying to failover to it Solution Installing ExacqVision server 64bit version

The failover is not working on the EM, and the protected server is stuck on Failed over however, the spare server is still on standby mode.

Issue The failover is not working on the EM, and the protected server is stuck on Failed over however, the spare server is still on standby mode. When checking the EM logs, it shows. Solution This issue has been fixed on Exacq EM version 22.09.2.0 or newer.

Enterprise Manager Failover

Enable automatic system failover to prevent loss in recording when an ExacqVision server loses network connectivity or is brought down for maintenance. Learn how to create a failover group for automated failover, perform a manually triggered failover, and how to failback to the original state.